The attempted command cannot be executed as messaging to the target axis failed
The online command failed because the messaging mechanism to the motion module failed. Retry the command. If the problem persists, check module connections, etc..
Provide Feedback