The servo module associated has faulted. Reset the fault and retry
The servo module has faulted. Check drive fault connections, for example, to determine the cause of the drive fault, clear the fault, and then retry the command.
Provide Feedback