Loading
Blog | Machine and Equipment Builders
Recent ActivityRecent Activity
4 minute read

It’s Time to Rethink Machine Safety and Security

More productivity. Less risk. Smart safety and CIP Security strategies can help OEMs meet the challenges of The Connected Enterprise head-on.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Operators in PPE with tablet

Digital technology continues to transform manufacturing. And as smart factory initiatives escalate, OEMs face new demands for highly productive, information-enabled machines that support digital transformation – and help maintain safety and security in a connected world.

Not so long ago, “productivity,” “safety” and “security” were viewed as separate machine considerations – often at odds with each other. However, in modern connected plants, they are indelibly linked. A security breach on an industrial control system can delay production, damage equipment, injure workers or harm the environment.

As a machine builder, you play a key role in helping manufacturers capture the benefits of connectivity – and mitigate risk. Thanks to new technologies – like smart safety and CIP Security – you can rethink your approach to machine design and step up to the challenge.

Smarter Devices. Smarter Safety.

Of course, machine safety has always been a critical consideration in your designs. But conventional machine safety systems provide little or no data.

For example, the system can notify an operator that a line has stopped, but cannot provide any information regarding the position or nature of the fault. So even an easily corrected safety fault – like a guarded access door being slightly ajar – can result in extensive troubleshooting and lost production time.

The key to smart safety – and better machine productivity – is more information. Smart safety takes advantage of digital technology and network connectivity to provide rich data that can optimize performance.

Simply put, smart safety controllers and devices acquire and process data – and can monitor and report on asset conditions in real time. They can communicate on the same EtherNet/IP™ network that runs the rest of the machine using a safety-based communication protocol – or built-in CIP Safety™ functionality, like this light curtain

.

Smart safety devices provide diagnostic information that can deliver valuable insights, such as exactly where a safety-related failure is occurring or if workers are following standard operating procedures. What’s more, smart safety devices enable better visibility into operations – and deliver the information manufacturers need to make better decisions about how to improve their processes.

The result? Faster troubleshooting. More machine uptime. Higher throughput.

Safety and Security – A Critical Relationship

There’s no doubt about it. In today’s increasingly connected plants, cybersecurity also impacts safety and productivity. A bad actor who infiltrates an industrial control system can quickly cause devastating damage – from manipulating a process to compromising a safety system.

At the same time, more manufacturers are looking for ways to enable secure remote access to their equipment. Indeed, one lasting lesson from the COVID-19 pandemic is that remote access can be critical when on-site service options are limited.

The good news? Cybersecurity is a foreseeable safety issue – and risk mitigation is attainable. In fact, a cybersecurity strategy based on defense-in-depth is one of the most effective measures manufacturers can take to help protect their systems. And your machine designs can support their efforts.

Keep Security in Mind as You Design

Ultimately, cybersecurity risk mitigation is dependent on the defense-in-depth strategy implemented by your customers. Specifically, the IEC 62443 standard provides the framework to address and mitigate security vulnerabilities in industrial automation and control systems (IACS).

To mitigate risk, manufacturers must focus on strong policies, physical protections, network infrastructure and segmentation, and securing their equipment. At the outset, they must first define how secure their machines are – and many are demanding equipment that meets more stringent security protocols.

How can you meet your customers’ cybersecurity expectations? Design your machine control systems with security in mind. Your first step is verifying that the control system components you apply feature robust security profiles designed for industrial environments and in compliance with IEC 62443.

Make Your Machines CIP Security Ready

While your customers will no doubt use a variety of methods to help thwart cybersecurity threats, CIP Security

™ is becoming an increasingly important way to reinforce a defense-in-depth strategy. To support this strategy, you can make your equipment “CIP Security ready.”

CIP Security helps provide a secure way to transport data – at the protocol level – on EtherNet/IP networks. A CIP Security enabled device can help protect itself from malicious communications in three important ways:

  • Rejects messages sent by untrusted people or untrusted devices
  • Rejects data that has been altered
  • Helps prevent viewing of EtherNet/IP data by unauthorized parties

The most vulnerable access point to your machine is its workstation which always links to the control system. To help mitigate that risk, an increasing number of controllers, drives and communication modules have built-in CIP Security capability.

To improve access control, you can group devices with CIP Security within your machine – and create a “zone” or set of devices that share the same security policy.

What about machine control devices without built-in CIP Security? Typically, these components are “allow listed” to communicate with devices within the zone. But now you can achieve an even higher level of machine protection, thanks to this new CIP Security proxy

.

A standalone hardware solution, the proxy is designed to help protect many of the EtherNet/IP control devices in use that don’t have built-in CIP Security capabilities. As a result, you can improve security not only in your new equipment designs, but in existing installations, too.

Learn more about how you can apply smart machine

strategies to help mitigate safety and security risk, improve uptime – and differentiate your offerings.

Steve Ludwig, Global Portfolio Manager, Integrated Architecture also contributed to this blog post.

Published March 29, 2021

Topics: Machine & Equipment Builders CIP Security Safety Solutions
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended for You

Learning+ TechConnect Genius Webinar: Introduction to FactoryTalk Design Studio
Upcoming
On-Demand
Learning+ TechConnect Genius Webinar: Introduction to FactoryTalk Design Studio
Event (Webinar)
Build Faster and Smarter with FactoryTalk Design Studio
Date: July 24, 2025
Time: 11:00 A.M. Central Daylight Time
Language: English
Smart Machines eBook
Smart tools displayed using futuristic neon circles with a dark blue background and a lighting effect
Brochure
Smart Machines eBook

Are you ready to "Get Smart"? Find out key considerations for developing smart machines and equipment.

Download Now
Smart Safety Interactive Brochure
Smart Safety Interactive Brochure
Brochure
Smart Safety Interactive Brochure

This interactive brochure shows how our Smart Safety products are integral to The Connected Enterprise® and how they can help enhance safety while optimizing your production and maintenance.

Discover How
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left It’s Time to Rethink Machine Safety and Security Chevron RightChevron Right