Mining companies are digging deeper than ever. And to maximize output, what starts as a pit mine often extends underground.
“As mines get deeper, extraction of valuable ore becomes more costly,” said Derek Meloche, manager of business development, Variant Mining Technologies. “In addition, safeguarding personnel from underground hazards is a critical concern.”
Located in the Sudbury basin in Ontario, Canada, Variant Mining Technologies specializes in solutions for underground hard rock mining. The company works to solve one of the industry’s biggest challenges – moving material underground safely and efficiently.
Opportunity at Massive Mongolian Mine
Recently, a leading global mining company engaged Variant Mining to solve an ore transport challenge for a copper and gold mine in Mongolia. The mining company began open pit mining at the site in 2011 and recognized the value that lay deep underground.
“In fact, this site boasts one of the largest known copper and gold deposits in the world,” Meloche said. “Specifically, the company approached us to design an ore-pass loading system for underground operations slated to begin in a few years.”
Upon completion, the underground mine is expected to produce 95,000 tonnes of ore per day, tripling the current production at the site.
Block Caving Challenges
Transporting ore underground presents significant challenges, depending on the excavation method used. Underground operations at the Mongolian mine will use the “block caving” method. In block caving, a large section of rock is undercut. The ore then collapses – or “caves” – gradually under its own weight.
The resulting rubble funnels through a series of vertical ore passes at various levels in the mine. A chute system is located at the bottom of each ore pass.
“The chute is a device that allows ore to be transferred safely to the haulage vehicles,” Meloche explained. “It controls the flow so haulage equipment can be loaded quickly and safely.”
Trucks collect the material from a chute at the haulage level and transport it to conveyance systems, which bring the ore to the surface.
If ore is not sufficiently controlled, loading material at the haulage level poses a significant safety risk to personnel. Potential hazards include chute failures, falling debris, uncontrolled run of muck and unexpected vehicle traffic.