By Leah Shenold, lockout/tagout engineer, Rockwell Automation
Lockout/tagout (LOTO) procedures are designed with the safety of maintenance professionals in mind, but they also consider workers who are around or operate machines. For instance, OSHA cited an automation company for nine violations in connection with a worker’s fatal injuries when the worker was caught and pinned by a conveyor that had lowered during a power-down process. He died about a week later. Two of the nine violations related to their failure to implement an effective LOTO program for machines’ energy sources and to train workers on proper procedures.
And that’s just one example of thousands of LOTO-related accidents that happen every year, sadly. Because multiple audiences need to read procedures, it’s important to be intentional about the information provided within each LOTO procedure and how it’s presented.
According to Occupational Safety and Health Administration (OSHA) regulation 1910.147, LOTO procedures “shall clearly and specifically outline the scope, purpose, authorization, rules, and techniques to be utilized for the control of hazardous energy, and the means to enforce compliance.” This means that each procedure should be clear and concise about the following things:
- Which piece of equipment the procedure pertains to.
- Who is qualified and allowed to perform the LOTO.
- The steps to be taken to perform LOTO properly.
- What the consequences will be if someone does not follow the LOTO procedure.