Complete integration in Logix Designer for safety, motion and control
MILWAUKEE, Nov. 6, 2014 — Rapidly changing consumer demands require machine and equipment builders to reduce development and installation time while increasing machine flexibility. The Allen-Bradley Kinetix 5500 servo drive with integrated safety can help machine builders satisfy those requirements by taking advantage of a single EtherNet/IP network, as well as a common design environment with Rockwell Software Studio 5000 Logix Designer software.
“Production requirements are constantly changing for end users in the packaging, converting and material-handling industries, meaning their safety requirements may change as well,” said Mike Schweiner, product manager, Rockwell Automation. “Putting safety on the network eases the configuration of and updates to safety functions. This allows machine builders to be very flexible with their design and differentiate themselves in these industries, providing customers the means to more easily react to market changes.”The Kinetix 5500 servo drive with integrated safety builds on the foundation of the recently released Kinetix 5500 servo drive. With the same high-speed coordination to meet demanding motion requirements, the drive uses the EtherNet/IP network for streamlined machine safety functions. End users gain the benefit of improved personnel safety and increased machine uptime in the manufacturing facility.
The EtherNet/IP network allows safety signals to travel via the same wires and IP addresses used for control and motion. This eliminates the need for a hardwired safety system. Reducing overall system wiring saves time and money in installation and removes potential points of failure, resulting in less troubleshooting and downtime.
Machine and equipment builders can more quickly install the drive and provide customers with greater ease of use via the Logix Designer development environment and Allen‑Bradley GuardLogix safety controllers. In addition to motion and control parameters, end users now can configure the safety system within the Logix Designer software. They can unlatch the safe torque off function, program an unlimited number of set points, change safety zoning, and re-use code to maintain system validation – all within a single software application.
End users also gain improved diagnostics information through the drive’s integration with the GuardLogix safety controller. Details on safety-related faults, such as safe torque off requests, are shown on the drive’s LCD display. This information can also be pulled into existing information databases and reporting solutions already in use, to deliver actionable safety information to users when and where they need it.
News Release Assets
Image available upon request or here at box.com.
About Rockwell Automation
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs about 22,500 people serving customers in more than 80 countries.
Media Contacts
Cheryl Abler
Rockwell Automation
414.382.1385
clabler@ra.rockwell.com
clabler@ra.rockwell.com
Marnie Kopischke
PadillaCRT
612.455.1737
marnie.kopischke@padillacrt.com
Allen-Bradley, GuardLogix, Kinetix, LISTEN. THINK. SOLVE. Rockwell Software and Studio 5000 are trademarks of Rockwell Automation Inc.
EtherNet/IP is a trademark of ODVA Inc.
Published November 5, 2014