Configure Sensors
After adding an Asset, the sensor details are auto populated, and the user is not allowed to add or delete sensors from the table.
Perform the following steps to edit the sensor details:
- Select the required sensor checkbox from the sensors table.
- ClickEdit.Edit Sensor Details
- Edit the required fields in theBasic details,Configure Tag,Configure Sensor Limitstab and clickSave.Basic DetailsConfigure TagConfigure Sensor Limits
The "
Sensor details were updated successfully
" message is displayed.
NOTE:
Click the required Sensor Name in the table to view the sensor details.
Provide Feedback