Asset Class

Asset Class

The user can view, add, edit, and delete the asset class. The following are the two types of asset classes:
  • User-Defined (Defined manually by a user)
  • Pre-Defined (Auto populated)
NOTE:
The user cannot add, delete, or modify the pre-defined Asset Class.

Add Asset Class

Perform the following steps to add an asset class:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Class Setup
    .
  2. In the
    Asset Class
    tab, click
    Add
    .
    Add Asset Class
  3. In the
    Class Definition
    tab, set these parameters:
    • Class Name
      : Provide the Class Name details.
    • Class Description
      : Provide a description for the class.
  4. Click
    Next
    .
    Class Definition
  5. In the
    Configure Sensors
    tab, set these parameters:
    • Sensor Name
      : Provide the Sensor Name details.
    • Sensor Description
      : Provide a description for the sensor.
    • Unit of Measure
      : Select the required Unit of Measure from the drop-down list.
    • Date Type
      : Select the required Date Type from the drop-down list.
  6. (Optional) Click the [+] icon to add a new row and repeat the previous step to configure more sensors.
    NOTE: To delete the configured sensor, click the [] icon.
  7. Click
    Next
    .
    Configure Sensors
  8. In the
    Configure Component Class
    tab, set these parameters:
    • Component Class Name
      : Select the required Component Class Name from the drop-down list.
    • Component Class Description
      : It is auto-populated based on the component class selection.
  9. (Optional) Click the [+] icon to add a new row and repeat the previous step to configure more component classes.
    NOTE:
    To delete the component class, click the [] icon.
  10. Click
    Add
    .
    Configure Component Class
    The “
    Asset Class Name was added successfully
    ” message is displayed.

Edit Asset Class

Perform the following steps to edit the asset class:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Class Setup
    .
  2. In the
    Asset Class
    tab, select the required Asset Class checkbox, and click
    Edit
    .
  3. Edit the required fields from the
    Class Definition
    ,
    Configure Sensors
    , and
    Configure Component Class
    tabs.
  4. Click
    Save
    .
    Asset Class Name was updated successfully
    ” message is displayed.
    NOTE: It is applicable only for User-defined Asset Classes.

View Asset Class

Perform the following steps to view the asset class:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Class Setup
    .
  2. In the
    Asset Class
    tab, click the required Asset Class Name to view the required details.

Delete Asset Class

Perform the following steps to delete the asset class:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Class Setup
    .
  2. In the
    Asset Class
    tab, select the required Asset Class checkbox, and click
    Delete
    .
  3. In the
    Delete Asset Class
    dialog box, click
    Delete
    .
    Delete Asset Class
    The “
    Asset Class Name was deleted successfully
    ” message is displayed.
    NOTE:
    • It is applicable only for User-defined Asset Classes.
    • If the Asset Class has associations, then the delete option is disabled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.