Integration Setup
Perform the following steps to integrate the setup:
- On the left navigation menu, drop-down theConfigurationmenu and clickCMMS Integration Setup.The Integration Setup tab is displayed.
- ClickEdit.
- In theCMMS Detailssection, Select the required CMMS application details from theChoose CMMS Applicationdrop-down list.
- In theIntegration Detailssection, provide the following details:NOTE: Use the API Application Key, Access Key, and API Secret from Fiix and have these credentials ready before starting the integration setup.
- API Application Key: Provide the application key details.
- Access Key: Provide the access key details.
- API Secret: Provide the API secret details.
- Fiix environment URL: Provide the environment URL details.
- API Application Key expiration date: Provide the API application key details.
- ClickTest Connection.If the connection is successful, then "Connection Established" message is displayed.
- In theIntegration Statussection, select the required duration time from theSync Time Durationdrop-down list.NOTE: The user can turn on theEnabledbutton to create a work order in Fiix.
- ClickSave.The user cannot save the connection, if the connection status is failed.
The timestamp is updated when the user navigates to this setup screen. The user can also view the last successful connection and unsuccessful connection timestamp details.
Integration Setup

Provide Feedback