Hierarchy Configuration

Hierarchy Configuration

Perform the following steps to configure
Weighted Average
for the selected node:
NOTE: The
Hierarchy Configuration
applies from the Region to the Sub-Area level.
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Dashboard Setup
    .
  2. Click the
    Hierarchy Config
    tab and the Hierarchy Config page is displayed.
    Hierarchy Configuration
  3. Click the required node from the hierarchy list.
  4. Click
    Edit
    .
  5. (Optional) In the
    Hierarchy Config
    tab, select the required
    Tag Name
    and
    Unit of Measurement
    from the drop-down lists.
    NOTE:
    The user can turn on the
    Enable KPI
    toggle button to view the throughput value in the cards.
  6. Provide the
    Child Weightage (%)
    value for all the child nodes.
    NOTE: The combined
    Weighted Average
    value of all child nodes must be 100%.
  7. Click
    Save
    .
    Hierarchy Config Page
    NOTE:
    Only Active child nodes are displayed in the table.
    The "
    Weighted Average has been edited successfully for the selected node
    " message is displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.