User-Defined Formulas
Add Formulas:
Perform the following steps to add user-defined formulas:
- On the left navigation menu, drop-down theConfigurationmenu and clickFormula Setup.TheUser Defined Formulastab is displayed.
- ClickAdd.
- In theBasic Detailstab, set these parameters:
- Formula Name: Provide the Formula Name.
- Version: Provide the Version details.
- Formula Description: Provide a description for the formula.
- Formula Status: Select the required status from the drop-down list.
- ClickNext.
- In theFormulaDetails tab, provide the formula in theEnter the Formula belowbox.
- ClickValidate.
- In the pop-up dialog, the user can view the formula in the book format and clickConfirm.
- After successful validation, underInput Variables Detailssection, set the following parameters for each name:
- Type: Select the required type (Variable or Constant) from the drop-down list.
- Unit of Measure: Select the required Unit of Measure from the drop-down list. It is applicable for Variables.
- (Optional)Description: Provide a description for the name.
- (Optional)Default Value: Provide a default value for the name and it is applicable for Constants.
- ClickNext.
- In theFormula Validationtab, perform the following actions:
- Provide the values to the input variables and clickTest Formula.
- The output value is displayed in theCalculated Outputbox.
- ClickSave.
The formula is added to the
User Defined Formulas
table. The Utilized in app
column is added to the existing table and it displays Yes
or No
based on the association with KPIs.dit Formulas
Perform the following steps to edit the formula:
- Select the required formula checkbox from the table.
- ClickEditand edit the required fields.
- ClickSave.
Delete Formulas
Perform the following steps to delete the formula:
- Select the required formula checkbox from the table.
- ClickDelete.TheDelete Formuladialog box is displayed.
- ClickDelete.The "Formula is deleted successfully" message is displayed.
Provide Feedback