Export Hierarchy/Asset
This functionality applies from Enterprise to Asset levels but not for the Component level. Perform the following steps to
Export Hierarchy
:- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Select the required node from the Hierarchy list.
- Click the [
] icon and select
Export Hierarchy.Export HierarchyNOTE: At the Asset level, the user views the Export Asset option instead of Export Hierarchy.
The selected node hierarchy is downloaded in Excel format and "
Node was exported successfully
" message is displayed. Export Hierarchy Template

Provide Feedback