Move Node
Perform the following steps to move the node:
NOTE:
This functionality is enabled only when the node's configuration status is in draft. The user can also move the node with its child elements only if both are in draft configuration status.
- On the left navigation menu, drop-down theConfigurationmenu and clickAsset Setup.
- Select the required node from the hierarchy list.
- Click the [
] icon and select
Move.Select Move Node - In theSelect Destinationdialog, select the required hierarchy level to move the selected node and clickMove.Select Destination"Node was moved under the node successfully" message is displayed.
Provide Feedback