Customer Onboarding Procedure
This onboarding process sets up Cognite Data Fusion (CDF) platform with data model and DataMosaix platform for credentials.
Customer Onboarding Procedure
:Once the prerequisites are met, the onboarding process begins automatically when the user launches the application for the very first time.
The process is repeated on every launch until the onboarding is done successfully.
On successful onboarding, dashboard is displayed. There will be no data presented in the application since no data source is configured.
NOTE:
In case of failure, the user will be requested to contact Rockwell Automation IT Administrator.
Provide Feedback