Roles and Permissions

Roles and Permissions

In this tab, the user can edit the existing roles and permissions and add new roles & users.
NOTE: By default, admin and unassigned roles are created with a new customer onboarding setup or tenant setup. The user can view only these two roles in the application.
Perform the following steps to edit the existing roles and permissions, add a user, and delete a user from the role:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    User Management
    .
  2. In the
    Roles and Permissions
    tab, select the required role from the
    Role List
    .
  3. In the
    Role Details
    section, click
    Edit Role
    .
  4. Edit the name and description of the role.
  5. In the
    Role Permissions
    section, select the required
    Dashboard Permissions
    and
    Configuration Permissions
    (
    Add
    ,
    Modify
    , and
    Delete
    ) checkboxes.
    Edit Role
  6. In the
    Active Users
    section, click
    Add User
    to add users to the role.
  7. In the
    Add User
    dialog, select the required
    User Name
    checkboxes and click
    Add User
    .
    Add User
  8. To delete a user from the role, click the [] icon on the required user.
  9. In
    Confirmation: Remove the user from the Role
    dialog, click
    Remove
    .
    Remove Confirmation Message
  10. Click [Save].
    The "
    Role has been modified successfully
    " message is displayed.
Perform the following steps to add a new role:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    User Management
    .
  2. Click
    Add Role
    .
  3. In the
    Add New Role
    dialog, under the
    Roles Details
    tab, set these parameters:
    • Role Name
      : Provide the role name.
    • Role Description
      : Provide a description of the role.
  4. Click
    Next
    .
    Role Details Tab
  5. In the
    Configuration Permissions
    tab, under
    Dashboard Permissions
    , select the required permission checkboxes.
  6. In the
    Configuration Permissions
    section, select the required permission checkboxes (
    Add
    ,
    Modify
    , and
    Delete
    ).
  7. Click
    Next
    .
    Configure Permissions tab
  8. In the
    Configure Users
    tab, select the required
    User Name
    checkboxes.
  9. Click
    Add
    .
    Configure Users
    The "
    Role has been added successfully to the role list for Asset Intelligence
    " message is displayed. The new role is added to the role list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal