Sites

Sites

In the Sites tab, the user can view the active user details of the available sites and add new users to the site. Perform the following steps to view, add, and delete users:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    User Management
    .
    The Roles and Permissions tab is displayed.
  2. Select the
    Sites
    tab.
    Select Sites tab
    The
    Site List
    is displayed in the left panel and the associated user details are displayed in the right panel.
  3. To add a user to the site, click
    Add User
    .
  4. In the
    Add User
    dialog, select the required
    User Name
    checkboxes and click
    Add User
    .
    Add User
    The "
    User has been added successfully to the user list for Asset Intelligence
    " message is displayed.
  5. To delete a user from the role, click the [] icon on the required user.
  6. In
    Confirmation: Remove the user from the Site
    dialog, click
    Remove
    .
    Remove User
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal