Advisory Alerts

An Advisory is generated when a failure is expected to occur within a certain time period, typically this is within 21 days. The Advisory contains information about the potential failure, including diagnostics and recommendations on how to validate and address the detected potential failure. Additional data is provided for context, a Snapshot tab allows user to view the current state of all the variables when the advisory was generated, and a Trend tab to allow user to analyze the advisory in more detail as required.
Advisories are generated on Asset Components. The following tabs are displayed in the advisory alerts:
  • Overview
  • Trends
  • Snapshot
Advisory Overview
Overview
In the
Overview
tab, there are four different sections such as Advisory Diagnostics, Advisory Summary, Advisory Action, and Work Order.
The
Advisory Diagnostics
section provides information about the potential failure, including the diagnostic and recommendations on how to validate and address the detected potential failure. If previous Diagnostics are provided on this component and it is displayed in the
Previous Diagnostic Details
section.
The
Advisory Summary
section provides advisory summary details along with current, and future risk scores and remaining useful hours of KPIs.
In the
Advisory Action
section, with appropriate user privileges, the user can change the status of the Status, Add Comments, and Upload associated files.
In the
Work Order
section, the user can create work order number, change status and add comments to the work order.
The
Work Order
section allows for the manual tracking of the associated Work Order required for the action of the alert.
  • Work Order No
    : Provide the work order number for the alert.
  • Work Order Status
    : Select the status from the drop-down list.
  • Comments
    : (Optional) Provide the comments for the alert as required.
NOTE: Click
View History
to view the history of changes that happened in the
Sensor Fault Action
and
Work Order
section.
View History
Trends
In the
Trends
tab, the user can view all associated parameters to the Component to do further analysis. The user can use the Select Parameter, Frequency, and Aggregation drop-down lists to filter the data.
Advisory Trend Tab
In the Trend, the user can view the Trend at the top and a sparkline view at the bottom. The user can change the date selection by using the selectors of 1/3/6 months, year to date [YTD], 1 year, and all. The user can use the sliding selector at the bottom to change the date selection.
Hover over the trend chart to view the parameter value with the corresponding date and time details.
Snapshot
The snapshot shows the condition of each sensor relative to the Advisory Threshold Limits at the time of the triggered Advisory.
There are two different types of Sensors Physical and Virtual as defined during the Asset Setup. The timestamp is provided as a starting point for additional investigations.
Advisory Snapshot Tab
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.