Area Level Dashboard
In this dashboard, the user can view the overview of the Area. Based on the configuration, the respective KPI details are displayed in the
Overview
tab in the form of cards.Select the required
Area
from the hierarchy list and the following tabs are displayed in the dashboard:- Overview
- Areas
- Assets
NOTE:
To change the date or time period, refer to Change Date or Time Period.
Overview
The user can view the status of the Area and the configured KPIs across the application under the selected Area and the top five underperforming assets on the selected time frame. The user can also view the active alerts with severity, actions taken, and the current status of the alert.
Area Overview

In the KPI trend chart, three lines indicate the three different KPI data, the solid lines indicate the historic data, and the dotted line indicates the extrapolated future projected data. Hover over the solid line and dotted line to view the KPI values with the corresponding date.
In the KPI trend chart, the user can view the Trend at the top and a sparkline view below. The user can change the date selection by using the selectors of 1/3/6 months, year to date [YTD], 1 year, and all. The user can use the sliding selector at the bottom to change the date selection.
NOTE:
- Click the [
] icon in the chart and click
Download SVG vector imageto download the chart in SVG vector image format. - Click the [
] icon in the chart and click
View in full screento view the chart in full screen.
The user can view the individual KPI graph of the
Top 5 Underperforming Assets
and the graph is displayed for the past 3 months. Hover the mouse over the chart to view the selected KPI value with the corresponding date. The user can also select the required KPI from the KPI drop-down list and the corresponding graph are displayed in the Past 3 Months
column.Top 5 Underperforming Assets

NOTE:
To customize the top 5 underperforming asset table, refer to Customize Top 5 Underperforming Assets Table.
Click the [
] icon on the required

Asset Name
to view the Asset Hierarchy
details.Asset Details

The user can view all the active alerts with alert descriptions, severity, start date, action taken, and current status details.
Active alerts

NOTE:
To customize the table, refer to Customize Table.
Areas
The user can view the status of the Sub Area on the Area. Each Area, for example, Milling has associated KPIs of Health Index, Reliability, Throughput, and Alert count. The associated KPIs are configured in the dashboard setup and the same KPIs are across the application.
Sub Area Cards

NOTE:
To know about the card functionality, refer to Card Functionality.
Assets
The user can view summaries of the asset classes associated with this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual
Asset Class
, the user can filter the list of assets available in the Asset Details
section. Click on the Asset Name
to view the corresponding Asset page.Asset Cards and Details

Provide Feedback