Asset Level Dashboard
In this dashboard, the user can view the overview of the Asset. Based on the configuration, respective KPI details are displayed in the
Overview
tab.Select the required
Asset
from the hierarchy list and the following tabs are displayed in the dashboard:- Overview
- KPIs
- Sensors
- Info
NOTE:
To change the date or time period, refer to Change Date or Time Period.
NOTE:
To customize the table, refer to Customize Table.
Overview
The user can view the status of the Asset and the configured standard KPIs under the dashboard setup and the component health with the health score, remaining useful Life, and alert count details. The user can also view the active alerts with severity, actions taken, and the current status of the alert.
In the KPI trend chart, three lines indicate the three standard KPI data, the solid lines indicate the historic data, and the dotted line indicates the extrapolated future projected data. Hover over the solid line and dotted line to view the KPI values with the corresponding date.
In the KPI trend chart, the user can view the Trend at the top and a sparkline view below. The user can use the sliding selector at the bottom to change the date selection.
Predictive Elements | Definitions |
---|---|
Health score | For a given Asset, Asset Health Value is calculated as Average of all the respective components' Health score. |
Remaining useful Life | For a given Asset, Asset RUL Value is calculated as Lowest of all the respective components' RUL score. |
NOTE:
- Click the [] icon in the chart and clickDownload SVG vector imageto download the chart in SVG vector image format.
- Click the [] icon in the chart and clickView in full screento view the chart in full screen.
The user can view all the
Active Alerts
of both Asset and Component levels rolled-up to the Asset. The following are three different types of alerts with respective hierarchy location applicability and links to additional information in the document: Alert type | Hierarchy Location | Links to Additional Information |
---|---|---|
The user can view the health of the components configured under the Asset with a health score, remaining useful hours, and alert count.
KPI
The user can view the KPI Alert history and the configured KPIs to the Asset for the applicable time period. The KPI alert history shows all KPI Alerts. Click on the
KPI Alert ID
to view more details on the KPI alerts.Click on any
KPI
, for example, the following image displays the Efficiency KPI and the user can view how the KPI has been performing over time, against the configured limits. For more details, view the Configuration
section.In the trend chart, the user can view the trend at the top and the sparkline view at the bottom. The user can also use the sliding selector at the bottom to change the date selection. The trend chart is displayed in three different tabs.
- Short Term: This trend chart displays the forecasted values for the next two weeks and the time resolution is one data point per hour.
- Long Term: This trend chart displays the forecasted values for the next two months and the time resolution is one data point per hour.
- Custom: The trend chart is displayed for the custom date selected in the From and To box using the date picker.
The red horizontal lines indicate the configured KPI Alert thresholds of Low, Medium, and High for the Upper and Lower thresholds. The following table provides additional information on the thresholds and the abbreviations used in the graphic.
Alert Severity | Alert Lower Limits | Alert Higher Limits |
---|---|---|
Low | LAL | LAU |
Medium | MAL | MAU |
High | HAL | HAU |
Sensors
In this tab, the user can view the sensor fault history, and sensors details.
In the
Sensor Fault History
section, the user can view all sensor faults based on the selected time period. Click on any Sensor Fault ID
to view the details of the sensor fault alerts.In the
Sensors
section, the user can view the sensors list with description, Data availability%, Valid data %, Unit of measure, Association, and Past 30 days trend.In the trend chart, the user can view the trend at the top and the sparkline view at the bottom. The user can also use the sliding selector at the bottom to change the date selection. The trend chart is displayed in three different tabs.
- Short Term: This trend chart displays the forecasted values for the next two weeks and the time resolution is one data point per hour.
- Long Term: This trend chart displays the forecasted values for the next two months and the time resolution is one data point per hour.
- Custom: The trend chart is displayed for the custom date selected in the From and To box using the date picker.
The red horizontal lines indicate the configured KPI Alert thresholds of Low, Medium, and High for the Upper and Lower thresholds.
Info
The user can view the general and system information about the Asset.
Provide Feedback