Region Level Dashboard
In this dashboard, the user can view the configured hierarchy elements that are child elements of the Region. Based on the configuration, the respective Product or Site details are displayed in the
Overview
tab as cards.Select the required
Region
from the hierarchy list and the following tabs are displayed in the dashboard:- Overview
- Sites
- Assets
NOTE:
To change the date or time period, refer to Change Date or Time Period.
Overview
The user can view the status of each element of the hierarchy available under
Region
. For example, Iron Ore has associated KPIs of Health Index, Reliability, Throughput, and Alert count. The associated KPIs are configured in the Dashboard Setup and the same KPIs are across the application. The KPI values are rolled up according to the hierarchy, with Alerts and KPI values originating in each asset and rolling up accordingly. The user can also view the top five underperforming assets. All of these are based on the selected time frame selectable in the top right corner of the dashboard.
Region Overview

NOTE:
Click the [>], [>>] and [<], [<<] paginator icons in the summary to move forward and backward to view the data.
NOTE:
To know about the card functionality, refer to Card Functionality.
The user can view the individual KPI graph of the
Top 5 Underperforming Assets
and the graph is displayed for the past 3 months. Hover the mouse over the chart to view the selected KPI value with the corresponding date. The user can also select the required KPI from the KPI drop-down list and the corresponding graph are displayed in the Past 3 Months
column.Top 5 Underperforming Assets

NOTE:
To customize the top 5 underperforming asset table, refer to Customize Top 5 Underperforming Assets Table.
Click the [
] icon on the required

Asset Name
to view the Asset Hierarchy
details.Asset Hierarchy details

Sites
On this tab, the user can view the associated sites that are under this point in the hierarchy. Each card represents an individual site, with the corresponding KPIs.
Site Cards

Assets
The user can view summaries of the asset classes associated with this point in the hierarchy. Each card represents an Asset Class with rolled-up statuses. By selecting an individual
Asset Class
, the user can filter the list of assets available in the Asset Details
section. Click on the Asset Name
to view the corresponding Asset page.Assets Cards

Provide Feedback