Asset Intelligence Features

Features List
S.No
Features
Description
1
Asset Intelligence Dashboards
It helps the user to visualize the KPI health, get the top 5 underperforming asset at all levels, and access the triggered alerts at each node.
2
Favorites
It helps the user to have a list of nodes added to favorites for easy access or navigation.
3
Compare
It helps the user to compare assets within an asset class and analyze their common and uncommon KPI Health and their component's risk score.
4
Underperforming Assets
It helps the user to analyze the top 5/10/20/100 underperforming assets across any level in the hierarchy considering their common KPIs.
5
Trending
It helps the user to visualize the Sensors or KPI's health and get useful insights from their data.
6
Alerts
It helps the user to navigate to the global alerts page with list of KPI alerts, Sensor fault alerts across all the levels in the hierarchy.
7
Data Source Onboarding [Configuration]
It helps the user to create FactoryTalk DataMosaix Extractors that simplifies the Data Source Onboarding Process.
8
Asset Setup [Configuration]
It helps the user to create an asset hierarchy structure, configure sensors and KPIs at the asset and component level.
9
Formula Setup [Configuration]
It helps the user to create User-Defined Formulas and view the Pre-Defined Formulas available.
10
Notification Setup [Configuration]
It helps the user to configure notification for an asset or asset group.
11
Dashboard Setup [Configuration]
It helps the user to configure default KPIs to be dis­ played on the cards throughout the application.
12
Class Setup [Configuration]
It helps the user to Create, Modify and Delete Asset and Component Classes.
13
User Management [Configuration]
It helps the user to create roles, manage user access and resources such as asset class and Sites.
14
User Settings
It helps the user to configure language settings.
15
Modifying the Hierarchy
It helps the user to modify the hierarchy structure by moving the hierarchy node.
16
CMMS Integration Setup
It helps the user to integrate Work Order generation by Asset and tracking in the Work Order progress in the CMMS.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.