Overview

Asset Intelligence is an application that aims to help customers improve the availability and reliability of their critical assets by actively monitoring the Health and Performance of those assets and notifying key stakeholders when action is needed to prevent planned and unplanned downtime.
Asset Intelligence is a Rockwell Automation Software-as-a-Service offering. It is accessible through the FactoryTalk Hub, and the Data Operations platform is FactoryTalk DataMosaix. All data that is needed as input for Health and Performance is available in FactoryTalk DataMosaix, where it can be easily consumed by Asset Intelligence.
Starting with the Mining Industry, pre-built Asset Classes are available for Ball Mills, Compressors, Conveyors, Crushers, Fans, Flotation Cells, Heat Exchangers, Pumps, Thickeners. These Asset Classes will provide users with value out of the box. Users can build out the hierarchy as required, applying Asset Classes to created Assets to shorten the time to value. The pre-defined KPIs, Asset Classes and the ability to define your own Asset Classes, Formulas and KPIs provide additional capability to expand and scale the solution further.
This user manual provides the information about how to use the application, configure, and interact with Asset Intelligence. It is divided into three sections:
  • Dashboards
  • Configuration
  • Tools
Additional references are also provided where applicable for interacting with other applications to ensure that the user can be successful with Asset Intelligence.
Asset Intelligence Overview
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.