Active Alerts
The user can view the alerts related to all the nodes. There are two types of alerts: Active and Historical Alerts.
Perform the following steps to view the
Active Alerts
:- On the left navigation menu, clickAlerts.TheActive Alertstab is displayed.
- Select the required node from the Hierarchy list.In theActive Alertstab,Sensor Fault, andKPI Alertcounts are displayed as cards. Click on a card to view the respective alerts in the table and click on theAlert IDto view the respective alert details.Active Alerts Tab
Provide Feedback