Historical Alerts
The user can view the alerts related to all the nodes.
Perform the following steps to view the Historical Alerts:
- On the left navigation menu, clickAlerts.TheActive Alertstab is displayed.
- Select theHistorical Alertstab.
- Select the required node from the Hierarchy list.In theHistorical Alertstab,Sensor Fault, andKPI Alertcounts are displayed as cards. Click on a card to view the respective alerts in the table and click on theAlert IDto view the respective alert details.Historical Alerts Tab
Provide Feedback