Compare Assets
The user can compare assets within the
Asset Class
and perform the following steps to Compare Assets
:- On the left navigation menu, clickCompare.TheAsset Comparisonpage is displayed.
- In theChoose Assetstab, set these parameters:
- Asset Class: Select the required Asset Class from the drop-down list.
- Region: (Optional) Select the required Region from the drop-down list.
- Product: (Optional) Select the required Product from the drop-down list.
- Site: (Optional) Select the required Site from the drop-down list.
- Area: (Optional) Select the required Area from the drop-down list
- (Optional) ClickApply Filter.
- Select the required asset checkbox and clickCompare Assets.NOTE:The user needs to select a minimum of 2 assets to a maximum of 4 assets to enableCompare Assets.In theSelectedtab, the user can view all the assets in the form of cards with all the KPI details configured under assets. The following sections are displayed in the asset cards.
- Asset Details
- Standard KPIs
- Common Asset KPIs
- Unique Asset KPIs
- Component Risk Score
- Asset Hierarchy Details
- In theSelectedtab, set these parameters:
- Asset KPIs: By default, all the Asset KPIs are selected. The user can select the required Asset KPI from the drop-down list.
- Components: By default, all the Components are selected. The user can select the required Components from the drop-down list.
- ClickApply Filter.By default, the user can view the Asset details, Standard KPIs, and Asset Hierarchy Details section if nothing is selected in the Asset KPIs and Components filters. Based on your selection, the cards section is updated.:NOTE: Select theSet as Standard Unit of Measurecheckbox on the required card to establish it as the master. The Unit of Measure in the Common Asset KPI section for the remaining cards is updated based on the master card.
- Click the [] icon to download the current result in PDF format.
- Click the [x] in the respective cards to remove the cards from theSelectedtab.
- Click the [] icon to expand and collapse the section.
Provide Feedback