Trending
Perform the following steps to view the trend chart:
- On the left navigation menu, clickTrending.The Trending page is displayed.
- ClickAdd Sensor/KPI.
- In theAdd Sensor/KPIwindow, set these parameters:
- Region: Select the required Region from the drop-down list.
- Product: Select the required Product from the drop-down list.
- Site: Select the required Site from the drop-down list.
- Area: Select the required Area from the drop-down list.
- Asset Class: Select the required Asset Class from the drop-down list.
- ClickApply.
- From the table, select the required Sensor/KPI checkbox and clickAdd Sensor/KPI.Add Sensor/KPI windowThe user can view the trend chart of selected Sensors and KPIs. By default, the trend chart is displayed for the past month. If you hover over any line in the chart, it shows the date, time, and KPI value.Trend ChartThe Trend Summary table displays the selected KPI/Sensor details, Tag type and Description, Min, Max, and Average value on the selected time period, Unit of Measurement (UoM), Asset, and Component details.Trend summary table
Provide Feedback