Create a change user form

Add a persistent login pane to the main window.
TIP: If you want to add a login page that disappears when you log in, see Develop a login page.
  1. From the
    FactoryTalk Optix Studio
    toolbar, select
    Template Libraries
    .
  2. In
    Libraries
    , search for
    Change User form
    .
  3. Under
    Components
    , drag
    Change User form
    onto
    UI
    in
    Project view
    .
  4. Select
    Close
    .
  5. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    ChangeUserForm1
    ChangeUserForm
    .
  6. In
    Properties
    , create a dynamic link between
    Users
    and
    ProjectName
    Security
    Users
    .
    For more information about dynamic links, see Create dynamic links.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.