Integrate the application interface with the script
Make the button trigger the label text change when you select the button.
- InProject view, selectButton1.
- InEvents, next toMouseClickEvent, selectand select .
- Create a dynamic link betweenlabelNodeIdandLabel1.For more information about dynamic links, see Create dynamic links.
Provide Feedback