Develop an interface that visualizes a periodic task

This interface visualizes a long-running task.
Application example
TIP:
You can download a sample project from:
ExampleApplication-PeriodicTaskVisualization.zip
Prerequisites
TIP: Do not set the project title to
PeriodicTask
. This is a reserved namespace.
In
FactoryTalk Optix Studio
, select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.