Connect to the OPC UA server
Connect to the OPC UA server by using UaExpert®.
- In UaExpert, select
.
- In theAdd Serverwindow:
- Expand the endpoint that you set inFactoryTalk Optix Studiofor the OPC UA server object and select theNonesecurity policy.
- InAuthentication Settings, select an authentication mode for the OPC UA server object settings.For example, if the nodes published by the server can be accessed only by a user, the user must be authenticated.
- SelectOK.The server is added to theProject.
- InProject, right-click the server and selectConnect.An untrusted certificate error message appears.
- SelectTrust Server Certificateand selectContinue.The certificate is considered trusted and the UaExpert client connects to the server.
- Once the server is stored in UaExpert, right-click the server and selectConnect.
Provide Feedback