Add a scale line pen
Add a scale line pen to visualize the distance between two variable values.
- InProject view, select or create anXYChartobject.
- Create two variables of theNumberdata type.For more information, see Variables.
- InProperties, next toPens, selectand selectScale line pen.
- Create dynamic links between theXandYproperties and the variables.For more information about dynamic links, see Create dynamic links.
Provide Feedback