Activate FactoryTalk Optix Runtime on online devices
Activate a Runtime entitlement through License Manager on a Runtime online device.
- Open License Manager using either the Windows Start menu or the icon on your desktop.
- SelectOnlineto activate a new entitlement on the Runtime device.
- SelectActivate an entitlement for this deviceandNext.Your entitlement key is a 25-character key created by FactoryTalk Optix used to allocate an entitlement to an organization.
- Access the FactoryTalk Optix landing page.
- Authenticate as required.
- SelectEntitlementsto view and copy the entitlement key.
- Enter the Entitlement Key and selectActivate.
- When the entitlement activates successfully, selectOK.
- SelectEntitlementsagain, and thenOrganization entitlementsto display the allocated entitlement.
NOTE:
When you deploy FactoryTalk Optix Applications to the Runtime device, all required Runtime files automatically deploy with the application.
The
Organization entitlements
page shows the following information about entitlements:
- Entitlement key
- User
- Contract Number
- Catalog Number
- Entitlement
- Purchase Date
- Expiration Date
- Activation Date
NOTE:
The
Purchase Date
corresponds to the Effective Date
column of the Entitlements
section in the FactoryTalk Hub. This is the date when the entitlement is available in FactoryTalk Hub and can be allocated to an organization.The
Activation Date
is the date when a user activated the entitlement.The
Expiration Date
occurs after the time that elapses between the Activation Date
and the entitlement duration.Provide Feedback