FactoryTalk Optix design environment
Interface Section | Description |
---|---|
A | Main toolbar |
B | Project panel displays project information model to display and set the structure of nodes. The nodes can be organized according to parent/child logics |
C | Types panels with details on:
|
D | Log panel displays messages related to the operation of the software |
E | Path of the object being edited in the editor |
F | Toolbar specific to the object type being edited |
G | Object editor to set interface objects or to configure other specific object types (such as tag importers or recipes) |
H | Properties panel displays the properties of the selected node in the Project or in the object editor |
I | Events panel to subscribe methods to events that can be generated |
Provide Feedback