Activate FactoryTalk Optix Runtime on online devices

Complete the Runtime entitlement online activation if the Runtime device is connected to the Internet.
NOTE: The entitlement serial number XXXXX-XXXXX-XXXXX-XXXXX-XXXXX is used in the following instructions as a placeholder.
  1. To allow for entitlement activation, launch the FTOptixEntitlementCli.sh, a self-installing shell script.
    NOTE: Only a superuser can install the FactoryTalk Optix Entitlement Manager CLI program for entitlement activation.
  2. In a terminal, enter
    sudo FTOptixEntitlementCli --onlineActivate --entitlementKey XXXXX-XXXXX-XXXXX-XXXXX-XXXXX
    .
  3. Enter
    sudo FTOptixEntitlementCli --showInstalledEntitlement
    to view entitlement details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.