Supported Libraries in FactoryTalk Optix
FactoryTalk® Optix™
supports libraries that ease application development with predefined faceplates, devices, and objects. The following libraries are supported:
- Power Device Library - For more information, see publication DEVICE-RM100
- Safety Device Library - For more information, see publication DEVICE-RM005
- Plex APM Library - For more information, see publication INFO-RM005
- Plex QMS Library - For more information, see publication INFO-RM006
- Fiix Library - For more information, see publication INFO-RM007
You can download the libraries at the Product Compatibility and Download Center (PCDC). The PCDC is available at: rok.auto/pcdc.
Provide Feedback