Configure an alarm event logger

Store logs about past events related to alarms in a database.
  1. In
    Project view
    , right-click
    DataStores
    and select
    New
    Embedded database
    .
  2. Hover-over
    EmbeddedDatabase1
    , select
    Edit
    , and enter
    AlarmDB
    .
  3. From the toolbar, select
    Template Libraries
    .
  4. In , search for
    Alarms Event Logger
    .
  5. Under
    Components
    , drag
    Alarms Event Logger
    onto
    Loggers
    in
    Project view
    .
  6. Select
    Close
    .
  7. In
    Project view
    , select
    AlarmsEventLogger1
    .
  8. In
    Properties
    , create a dynamic link between
    Database
    and
    ProjectName
    DataStores
    AlarmDB
    .
    For more information about dynamic links, see #.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.