- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Access the CST object
The coordinated system time (CST) object provides coordinated system time for the devices in one chassis.
Attribute | Data Type | Instruction | Description |
---|---|---|---|
CurrentStatus | INT | GSV | Current status of the coordinated system time. Each bit has a specific meaning:
|
CurrentValue | DINT[2] TIME32[2] TIME | GSV | Current value of the timer. DINT[0] contains the lower 32; DINT[1] contains the upper 32 bits. The timer source is adjusted to match the value supplied in update services and from local communication network synchronization. The adjustment is either a ramping to the requested value or an immediate setting to the request value, as reported in the CurrentStatus attribute. |
Provide Feedback