Interpret the Attribute Tables
Each attribute table begins with the attribute name as a heading. The tag, GSV/SSV, and MSG names for each of these attributes are the same as the attribute name listed, but with the spaces removed. For example, Inhibit Axis would be InhibitAxis.
This table provides an explanation of the information, nomenclature, and abbreviations used in the attribute tables.
Attribute Table Column Heading Descriptions
Column Heading | Description |
---|---|
Usage (Implementation) | The following identifiers are used for usage:
In the Usage column, you will also see combinations of Usage and Mode, such as the following: C PVT Closed Loop Vector Control Method D FC Drive (Any Frequency Controlled or Vector Controlled drive device) In addition to these combinations, there are many attributes that are applicable or not applicable to sensorless drive operation, for example, velocity-controlled drives operating without a feedback device. To accommodate these situations, the following Device Function Codes are used:
|
Device Control Codes (mode) | The following identifiers are used for Device Function Codes:
If applicable only to specific implementations, the following codes will be used to denote when they apply:
|
Access Rules | The following identifiers are used for the Access Rules:
|
T | Can be accessed as an Axis Tag |
Data Type | For example, DINT, UINT, SINT, REAL, BOOL |
Default, Minimum, Maximum Range Limits | DB = Motion Database Indicates that the default value comes from the database. FD = Factory Default computed value ∞ = max float = 3.402.... x 10 38 0+ = min float = 1.2.... x 10 -38 maxpos = 2 31 /Conversion Constantmaxspd = 1000 * maxpos minspd = minfloat maxacc = 1000 * maxspd minacc = minfloat maxint = 2 15 - 1maxdint = 2 31 - 1- (dash) = Not Applicable N/A = Not Applicable Defaults = Unless otherwise specified, all optional attributes default to 0. All reserved and otherwise unused bits and enumerations are set to 0. |
Semantics of Values | The meaning of the attribute values. For example: Position Units / Sec. Tag access is supported by value is valid only when Auto Tag Update of the Motion Group Object is enabled. There may be additional information in the description that directly follows the attribute listing. |
CST | Coordinated System Time |
Provide Feedback