Transition

Transition

The Transition determines if the controller goes on to execute the next step.
A Transition in a sequential function chart (SFC) is the true or false condition that tells the controller when to go to the next step. The transition defines the physical conditions that must occur or change in order go to the next step.
Available Languages
Ladder Diagram
Not Available
Function Block
Not Available
Sequential Function Chart
Transition
LogDesSFCTrans
Structured Text
Not Available
Operands
Sequential Function Chart
Operand
Type
Format
Description
Transition
BOOL
tag
a transition is the true or false condition that tells the controller when to go to the next step
Description
Each transition use a backing tag that uses the BOOL data type.
If the transition is
The value is
And
true
1
the controller goes to the next step.
false
0
the controller continues to execute the current step.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.