Connected To Go Online dialog box - Options tab
This dialog box provides information about why the
Logix Designer
application could not go online, and how to correct the problem. This dialog box also allows limited access to controller status information without requiring correlation with the controller.From this dialog box, browse for a specific project file to open (and subsequently download), or select the
Nonvolatile Memory
tab to load a project from nonvolatile memory. Once that is done, choose to go online or upload.Parameters
Condition
Describes the reason that the
Logix Designer
application could not go online with the controller.Refer to the topic
Correlate a Project with a Controller
for a list of all possible conditions.Connected Controller
Information about the connected controller includes:
- Controller NameThe name of the controller to which the software is connected.TIP:If there is currently no project downloaded to the controller, and there is no project open offline, then this field displays <no name>.
- Controller TypeThe controller type to which the software is connected.
- Comm PathThe communications path being used to connect to the controller.
- Serial NumberThe serial number of the Safety controller. This option is enabled for Safety controllers only.
- SecurityThe Security Authority bound to the controller. Refer to theController Propertiesdialog box,Securitytab to configure a Security Authority for a controller.
Offline Project
Information about the offline project includes:
- Controller NameThe name of the controller in the offline project file.
- Controller TypeThe controller type in the offline project file.
- FileThe name of the project file, including its full path. This field is blank if you did not have a project open to start with, and a project file with the name found in the controller was not found in your project directory.
- RevisionThe firmware revision for which the project is configured.
- Serial NumberThe serial number of the controller use in the offline project.
- SecurityThe Security Authority assigned for the controller used in the offline project.
Prohibit online edits during upload
Select this check box to prevent online edits in other instances of the project during project upload.
Upload
Select this button to start the Upload function to upload the connected controller into the open project file. When selected, you are prompted to save any changes made in the open file. When the upload occurs, documentation associated with objects in the controller is preserved; unused comments and descriptions are deleted.
If the upload is successful, the system goes online. If the upload fails, errors are listed in the Output window.
Download
Select this button to start the download process. If the download is successful, the application goes online. If the download is unsuccessful, an error appears, and the application returns to the offline state.
In either case, the dialog box closes.
Select File
Select this button to access the
Select File
dialog box to choose a different project file. Choose an existing file, or enter the name of a new file for the system to create and upload into.Provide Feedback