Save As dialog box
Use this dialog box to save the project file to a different file with a new name, or to perform a full export of the project file. To open the
Save As
dialog box, select >
TIP:
Saving the project as a new file does not change the name of the controller. To change the controller name, use the
General
tab of the Controller Properties
dialog box.This table describes the settings on the dialog box.
Setting | Description |
---|---|
Save in | Specify the directory in which to save this project or in which to export the project. |
File name | Enter the name for the saved or exported file. |
Save as type | Choose the type of file to save or the file to export:
|
Encode Protected Content | Exports protected content in encoded format. Routines and Add-On Instructions can be exported in an encoded format when protected with FactoryTalk Security and/or Source Protection.Enabled when choosing either .L5K or .L5X from the Save as type menu, and Always Encode Protected Content on Export in the Workstation Options dialog box is cleared.Select to export protected content in an encrypted format, even when source key or other credentials for the content are present. Clear to export protected content in clear text.
TIP:
When exporting a project, only controls the encoded export of protected components, such as routines or Add-On Instructions, that can be exported encoded.
TIP:
Protection permissions (such as permissions configured in FactoryTalk Security or Source Protection) can override this selection. When checkbox cleared, the component is still exported encoded even if no permission to export unencoded. |
Provide Feedback