Actions page
Use the
Actions
page to:- Configure how an axis responds to fault types.
- Modify actions for how an axis responds to fault types.TIP: Some of the options for each of the actions, such as the options for theDisable (MSF) Stopping Actioncontrol, may change depending on the axis configuration and information from the drive's profile.
TIP:
Top open the Actions page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickActions.
The parameters are separated into Standard Actions and Safety Actions.
Standard Actions parameters
Parameter | Description |
Disable (MFS) Stopping Action | Select the stop action for the motor. The options vary depending on the axis configuration type selected on the General page.If the Axis Configuration on the General page is set to:
|
Connection Loss Stopping Action | Specifies the stopping method applied to the motor when it detects a loss of connection. The available options include:
|
Converter Input Phase Loss Action | Specifies the converter's response to an incoming phase loss while the converter is running. The available options include:
|
Power Loss Action | Specifies the power loss action for the motor. Possible available options include:
|
Shutdown Action | Specifies the shutdown action of the motor. The available options include:
|
Motor Overload Action | Specifies the motor overload action for the motor. The available options include:
This field is optional. |
Inverter Overload Action | Specifies the inverter overload action for the motor. The available options include:
This field is optional. |
Drive Overload Action | Specifies the drive overload action for the motor. The available options include:
This field is optional. |
AC Line Frequency Change Action | Specifies the converter's action when the rate of change of the AC line frequency exceeds a hard-coded threshold or the configured frequency change threshold.
This field is optional for Regenerative Converters. |
AC Line Sync Loss Action | Specifies the converter's response to an incoming line synchronization loss condition while the converter is running.
|
AC Line Voltage Sag Action | Specifies the converter's response to an incoming AC Line Voltage Sag condition while the device is running.
|
Converter Overload Action | Specifies the device's response to a converter overload condition.
|
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.Tip: The Parameter List page may contain more attributes than the associated page. In some cases, attributes that display on the Parameter List page do not display on the associated page. |
Danger: Vertical Load is enabled. Changing Action attributes from the Current Decel & Disable setting could endanger personnel, machine, and property. | Displays warning when Vertical Load Control setting on the General page is set to Enabled . |
Safety Actions parameters
Parameter | Description |
---|---|
Safe Torque Off Action | Determines the stopping method to apply to the motor when the drive detects a Safe Torque Off (STO) Active condition that was not initiated by a Safe Stop 1 (SS1) Active condition, and Safe Torque Off Action Source is set to Connected Drive .The available options include:
|
Safe Torque Off Action Source | Specifies whether the drive or the controller initiates the stopping sequence in response to a Safe Torque Off Active condition. The available options include:
|
Safe Stopping Action | Specifies the stopping method that the drive is to apply to the motor. The available options include:
|
Safe Stopping Action Source | Specifies whether the drive or the controller initiates the stopping sequence in response to a Safe Stop Active condition. The available options include:
|
Danger: Selection of Running Controller requires the user program to execute stopping action. | This warning displays when Safe Stopping Action Source or Safe Torque Off Action Source is set to Running Controller . |
Provide Feedback