Next Destructive Reference command
Select the
Next Destructive Reference
command to navigate to the next occurrence of a destructive reference for a tag. This command is not available until you have used the First Destructive Reference
command. If an instruction can overwrite a tag value, the instruction is a destructive reference for that tag.
Provide Feedback