Customize the Language Element Toolbar
To customize the Language Element toolbar:
- From theLanguagemenu, choose the language of the toolbar you want to modify.
- Add and remove buttons to configure your toolbar.Select thearrowbuttons to add and remove toolbar buttons.
- SelectOKto accept your toolbar configuration.
- SelectCloseto close theCustomize Toolbar - Language Elementdialog box.
To access the Customize Toolbar - Language Element dialog box
To access the
Customize Toolbar- Language Element
dialog box, from the View
menu, choose Toolbars
.The Toolbars
dialog box opens. Select the Language Element toolbar
from the list. Select Customize
.The Customize Toolbar - Language Element
dialog box opens.
TIP:
If FactoryTalk Security is enabled, this dialog may be disabled, depending on the levels of access that have been defined. For details about FactoryTalk Security see FactoryTalk Help:
Start > Programs > Rockwell Software> FactoryTalk Help
.Provide Feedback