Data Type Editor

Data Type Editor

Use the
Data Type Editor
to create user-defined data types. A user-defined data type groups different types of data, called members, into a single structure. Define the members and assign each member a name to describe the data it holds. Access a member by referencing the tag name member.
TIP: To open the Data Type editor: In the Controller Organizer, expand the
Assets
folder, right-click the
Data Types
folder, and choose
New Data Type
, or double-click an existing data type in the Data Types folder structure.
Online editing is allowed for member names of user-defined data types on
CompactLogix
5380,
Compact GuardLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers. Editing member names online is disabled when using the:
  • Member in an Add-On Instruction sealed with a signature.
  • Data type on a safety tag and the controller is in the Safety Secured state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.