Did the axis move in the positive direction?

The Motor Test command requires you to observe the direction of axis motion when executed. Answering Yes confirms that the desired positive motion of the axis matched the direction of motion when Motor Test was executed; answering No confirms that the desired positive motion of axis is opposite to the direction of motion when Motor Test was executed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.