Configure X, Y arrays for Function Generator (FGEN) instructions
Use the
X, Y Arrays
tab on the Function Block Properties
dialog box to configure X and Y arrays for Function Generator (FGEN) instructions.
TIP:
To open the X, Y Arrays tab on the Function Block Properties dialog:
- In the Function Block Diagram editor, insert an FGEN function block.
- On the function block, select theConfigurationicon
, or right-click the function block and select
Propertiesfrom the context menu.
This table describes the parameters on the tab.
Parameter | Description |
Table 1 Array | Select the tags for X1 Array and Y1 Array for Table 1. These arrays must be at least as Table 1 - # elements required . This setting is controlled by the XY1Size parameter. Select the Parameters tab on the Properties dialog box to configure XY1Size . The values of the selected tag arrays appear in Table 1. |
Table 2 Array (optional) | Select the tags for X2 Array and Y2 Array for Table 2. These arrays must be at least as Table 2 - # elements required . This setting is controlled by the XY2Size parameter. Select the Parameters tab on the Properties dialog box to configure XY2Size . The values of the selected tag arrays appear in Table 2. |
New Tag | Click New Tag to create a new tag for an array. |
Status | Displays read-only status information for blocks containing status bits. If none of the status bits are set, an OK message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values. |
Execution Order Number | Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a Routine not verified message displays. Note that this item is read-only. |
Never display description in a routine | Select this check box to prevent the description from appearing in the routine. |
Provide Feedback