Go To dialog box settings

Use these settings on the
Go To
dialog box to navigate in the language editor, Tag Editor, Data Monitor, and
Equipment Sequence
diagram editor.
Setting
Description
Go to what
Select the item to which you want to navigate. The choices available depend on the language editor you are using when you open the
Go To
dialog box.
Place caret on rung
In the ladder editor, enter the rung number to which you want to go.
Place the caret on line
In the structured text editor, enter the line number to which you want to navigate.
Edit Properties Of
Choose the routine or
Equipment Sequence
for which you want to edit properties.
Move to grid location
In the In the Function Block, SFC, or
Equipment Sequence
diagram editor, type the coordinates (for example, B24) of the grid location to which you want to go.
Set row selection on tag
In the Tag Editor or Data Monitor, enter tag name of the row to which you want to navigate.
Auto Navigate
Select this checkbox to automatically navigate to the row of the tag in the Tag Editor as you type text in the
Set row selection on tag
field. Selecting
Auto Navigate
highlights the row of the tag as you type. If you do not select
Auto Navigate
, the row is highlighted when you click
Go To
.
Go To
After you choose your item, click
Go To
to go to that location.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.