View Multiple Routines at the Same Time
View multiple routines at the same time using separate window instances. If the same routine is open in more than one window, any change made to the routine is reflected in all windows.
To view multiple routines at the same time:
- From theWindowmenu, chooseNew Window.A second routine window opens with the same tabs as the active routine window.
- In the second window, select the tab of the routine to view.If opening another routine; it opens into the active window.
Provide Feedback