Monitor Equipment Phases command

Choose this command to see an overview of the equipment phases in the controller. Use this overview during system commissioning or troubleshooting to view the equipment phase execution and to take control of an equipment phase when sending commands to it.
Important:
This feature is disabled in this version of the
Logix Designer
application.
To monitor multiple equipment phases running at the same time, use the
Window>New Window
command to open multiple
Equipment Phase Monitor
. (Open one
Equipment Phase Monitor
before using the
Window>New Window
command to open additional
Equipment Phase Monitor
.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.